Property (Read-Write)
SCPI.CALCulate.FP(Ch).TRACe(Tr).MATH.FUNCtion = Value
Value = SCPI.CALCulate.FP(Ch).TRACe(Tr).MATH.FUNCtion
This command sets/gets Select math operation type, for the selected trace Tr of the selected channel Ch.
|
Parameter |
Value |
|
Description |
Math function operation |
|
Data Type |
Character string type (String) |
|
Range |
NORMal|SUBTract|DIVide|ADD|MULTiply|USER |
|
Preset Value |
NORMal |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as String
Var= "NORMal"
SCPI.CALCulate.FP1.TRACe4.MATH.FUNCtion = Var
Var = SCPI.CALCulate.FP1.TRACe4.MATH.FUNCtion
SCPI.CALCulate.FP(Ch).TRACe(Tr).MATH.FUNCtion
SCPI.CALCulate.FP(Ch).TRACe(Tr).MATH.MEMorize
SCPI.CALCulate.FP(Ch).TRACe(Tr).MATH.OFFSet
FP Menu: Trace View > Data Math
:CALCulate:FP[1-1]:TRACe[1-4]:MATH:FUNCtion {NORMal|SUBTract|DIVide|ADD|MULTiply|USER}
:CALCulate:FP[1-1]:TRACe[1-4]:MATH:FUNCtion?
{NORMal|SUBTract|DIVide|ADD|MULTiply|USER} <newline><^END>
10 OUTPUT 717;":CALCulate:FP1:TRACe4:MATH:FUNCtion NORMal"
20 OUTPUT 717;":CALCulate:FP1:TRACe4:MATH:FUNCtion ?"
30 ENTER 717;A$