Property (Read-Write)
SCPI.DISPlay.ECHO.STATe = Value
Value = SCPI.DISPlay.ECHO.STATe
This command Show/Hide echo window.
|
Parameter |
Value |
|
Description |
Show/Hide echo window |
|
Data Type |
Boolean type (Boolean) |
|
Range |
ON|OFF|1|0 |
|
Preset Value |
OFF |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
No |
|
Save-Recall Effect |
No |
|
Error |
- |
Dim Var as Boolean
Var= 1
SCPI.DISPlay.ECHO.STATe = Var
Var = SCPI.DISPlay.ECHO.STATe
PN Menu: Macro Setup > Echo Window Menu > Echo Window
SP Menu: Macro Setup > Echo Window Menu > Echo Window
FP Menu: Macro Setup > Echo Window Menu > Echo Window
TR Menu: Macro Setup > Echo Window Menu > Echo Window
AM Menu: Macro Setup > Echo Window Menu > Echo Window
BB Menu: Macro Setup > Echo Window Menu > Echo Window
USER Menu: Macro Setup > Echo Window Menu > Echo Window
:DISPlay:ECHO:STATe {ON|OFF|1|0}
:DISPlay:ECHO:STATe?
{ON|OFF|1|0} <newline><^END>
10 OUTPUT 717;":DISPlay:ECHO:STATe 1"
20 OUTPUT 717;":DISPlay:ECHO:STATe ?"
30 ENTER 717;A