Property (Read-Write)
SCPI.SENSe.DCONverter.MANual.IFDelta = Value
Value = SCPI.SENSe.DCONverter.MANual.IFDelta
This command sets/gets down converter delta IF frequency (IF2 - IF1).
|
Parameter |
Value |
|
Description |
Down converter delta IF frequency (IF2 - IF1) |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
-3G ~ 3G |
|
Preset Value |
0 |
|
Unit |
Hz |
|
Resolution |
1 |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= -1000000000
SCPI.SENSe.DCONverter.MANual.IFDelta = Var
Var = SCPI.SENSe.DCONverter.MANual.IFDelta
SCPI.SENSe.DCONverter.MANual.IFGain(1-2)
PN Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
SP Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
FP Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
TR Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
AM Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
BB Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
USER Menu: System > Instrument Setup > Downconverter Manual Setup > ÄIF = IF2 - IF1
:SENSe:DCONverter:MANual:IFDelta {-3G ~ 3G}
:SENSe:DCONverter:MANual:IFDelta?
{-3G ~ 3G} <newline><^END>
10 OUTPUT 717;":SENSe:DCONverter:MANual:IFDelta -1000000000"
20 OUTPUT 717;":SENSe:DCONverter:MANual:IFDelta ?"
30 ENTER 717;A