Property (Read-Write)
SCPI.SENSe.DCONverter.MANual.IFGain(1-2) = Value
Value = SCPI.SENSe.DCONverter.MANual.IFGain(1-2)
This command sets/gets down converter IF Gain.
|
Parameter |
Value |
|
Description |
Down converter IF Gain |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
0 ~ 35 |
|
Preset Value |
0 |
|
Unit |
dB |
|
Resolution |
5 |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= 0
SCPI.SENSe.DCONverter.MANual.IFGain2 = Var
Var = SCPI.SENSe.DCONverter.MANual.IFGain2
SCPI.SENSe.DCONverter.MANual.IFDelta
PN Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
SP Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
FP Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
TR Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
AM Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
BB Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
USER Menu: System > Instrument Setup > Downconverter Manual Setup > IF Gain 1
:SENSe:DCONverter:MANual:IFGain[1-2] {0 ~ 35}
:SENSe:DCONverter:MANual:IFGain[1-2]?
{0 ~ 35} <newline><^END>
10 OUTPUT 717;":SENSe:DCONverter:MANual:IFGain2 0"
20 OUTPUT 717;":SENSe:DCONverter:MANual:IFGain2 ?"
30 ENTER 717;A