Property (Read-Write)
SCPI.SENSe.DCONverter.MANual.MEXTernal(1-2).BIAS.CURRent = Value
Value = SCPI.SENSe.DCONverter.MANual.MEXTernal(1-2).BIAS.CURRent
This command sets/gets external mixer bias current.
|
Parameter |
Value |
|
Description |
External mixer bias current |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
-10m ~ 10m |
|
Preset Value |
0 |
|
Unit |
A |
|
Resolution |
10u |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= -0.01
SCPI.SENSe.DCONverter.MANual.MEXTernal2.BIAS.CURRent = Var
Var = SCPI.SENSe.DCONverter.MANual.MEXTernal2.BIAS.CURRent
SCPI.SENSe.DCONverter.MANual.MEXTernal(1-2).BIAS.STATe
PN Menu: System > Instrument Setup > Downconverter Manual Setup > Current
SP Menu: System > Instrument Setup > Downconverter Manual Setup > Current
FP Menu: System > Instrument Setup > Downconverter Manual Setup > Current
TR Menu: System > Instrument Setup > Downconverter Manual Setup > Current
AM Menu: System > Instrument Setup > Downconverter Manual Setup > Current
BB Menu: System > Instrument Setup > Downconverter Manual Setup > Current
USER Menu: System > Instrument Setup > Downconverter Manual Setup > Current
:SENSe:DCONverter:MANual:MEXTernal[1-2]:BIAS:CURRent {-10m ~ 10m}
:SENSe:DCONverter:MANual:MEXTernal[1-2]:BIAS:CURRent?
{-10m ~ 10m} <newline><^END>
10 OUTPUT 717;":SENSe:DCONverter:MANual:MEXTernal2:BIAS:CURRent -0.01"
20 OUTPUT 717;":SENSe:DCONverter:MANual:MEXTernal2:BIAS:CURRent ?"
30 ENTER 717;A