Property (Read-Write)
SCPI.SENSe.SP(Ch).CARRier.FBANd = Value
Value = SCPI.SENSe.SP(Ch).CARRier.FBANd
This command sets/gets carrier frequency band, for the selected channel Ch.
|
Parameter |
Value |
|
Description |
Carrier frequency band |
|
Data Type |
Character string type (String) |
|
Range |
LOW|HIGH|BAND3|BAND4 |
|
Preset Value |
HIGH |
|
Unit |
- |
|
Resolution |
- |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
When the E5052B is used stand-alone, or with the downconverter turned off, or with the downconverter on and the RF input is set to 'E5052B Direct'
|
Parameter |
<string> |
|
LOW |
Set the carrier frequency band to '10M-1.5GHz' |
|
HIGH ( Preset value) |
Set the carrier frequency band to '300M-7GHz' |
When the downconverter is turned on and the RF input is set to 'Downconverter'
|
Parameter |
<string> |
|
BAND3 (Preset value) |
Set the carrier frequency band to '3G-10GHz' |
|
BAND4 |
Set the carrier frequency band to '9G-26.5GHz' |
Dim Var as String
Var= "LOW"
SCPI.SENSe.SP1.CARRier.FBANd = Var
Var = SCPI.SENSe.SP1.CARRier.FBANd
SCPI.SENSe.SP(Ch).CARRier.SET.CENTer
SP Menu: Start/Center > Carrier To > Frequency Band
SP Menu: Stop/Span > Carrier To > Frequency Band
:SENSe:SP[1-1]:CARRier:FBANd {LOW|HIGH|BAND3|BAND4}
:SENSe:SP[1-1]:CARRier:FBANd?
{LOW|HIGH|BAND3|BAND4} <newline><^END>
10 OUTPUT 717;":SENSe:SP1:CARRier:FBANd LOW"
20 OUTPUT 717;":SENSe:SP1:CARRier:FBANd ?"
30 ENTER 717;A$