Property (Read-Write)
SCPI.SENSe.UDConverter.LO = Value
Value = SCPI.SENSe.UDConverter.LO
This command sets/gets user downconverter local frequency.
|
Parameter |
Value |
|
Description |
User downconverter local frequency |
|
Data Type |
Double precision floating point type (Double) |
|
Range |
10M ~ 330G |
|
Preset Value |
3G |
|
Unit |
Hz |
|
Resolution |
100m |
|
Preset Effect |
Yes |
|
Save-Recall Effect |
Yes |
|
Error |
- |
Dim Var as Double
Var= 10000000
SCPI.SENSe.UDConverter.LO = Var
Var = SCPI.SENSe.UDConverter.LO
SCPI.SENSe.UDConverter.HARMonic
PN Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
SP Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
FP Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
TR Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
AM Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
BB Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
USER Menu: System > Instrument Setup > Frequency Offset (User Downconv.) > LO Frequency
:SENSe:UDConverter:LO {10M ~ 330G}
:SENSe:UDConverter:LO?
{10M ~ 330G} <newline><^END>
10 OUTPUT 717;":SENSe:UDConverter:LO 10000000"
20 OUTPUT 717;":SENSe:UDConverter:LO ?"
30 ENTER 717;A