Other topics about Making Measurement
Select a measurement to be triggered using the :TRIGger:MODE command.
Set the trigger source of the triggered measurement to Internal using the :TRIGger:xx:SOURce command.
Set the continuous initiation mode of the enabled triggered measurement using the :INITiate:xx:CONTinuous command.
Select a measurement to be triggered using the :TRIGger:MODE command.
Set the trigger source of the triggered measurement to Bus using the :TRIGger:xx:SOURce command.
Set the continuous initiation mode of the enabled triggered measurement using the :INITiate:xx:CONTinuous command.
Trigger the instrument when you want to perform measurement. An external controller can trigger the instrument by only a single command.
|
Command |
Applicable |
|
*TRG |
Bus trigger only |
To start the next measurement cycle, repeat step 4.
You can make the E5052B repeat a cycle of waiting for a trigger and performing measurement for the number of times specified by the averaging factor with a single transition to the “Initiate” state. To switch between the averaging trigger mode and the normal trigger mode, use the following command.
• :TRIGger:AVERage
|
Averaging trigger mode |
State transition for each setting |
|
On |
Turns on the averaging trigger mode. The instrument repeats a cycle of "waiting for a trigger" to "performing measurement," as many times as specified by the averaging factor, and then transitions to the “Hold” state. |
|
Off |
Turns off the averaging trigger mode. When the instrument finishes a single cycle of “waiting for a trigger” to “performing measurement,” it transitions to “Hold” state. |
The following table shows the operational difference between the trigger systems.
|
Continuous initiation mode |
Averaging trigger mode |
Operation of trigger system |
|
Off (Single) |
Off |
The instrument waits for a trigger only once. When it receives a trigger, it performs measurement and then transistors to the “Hold” state. The averaging factor is not cleared; it is incremented. |
|
On |
The instrument repeats a cycle of “waiting for a trigger” to “receiving a trigger” to “performing measurement,” as many times as specified by the averaging factor, and then transitions to the “Hold” state. The averaging factor is cleared before the start of measurement after receiving the first trigger. |
|
|
On (Continuous) |
Off |
The instrument repeats a cycle of “waiting for a trigger” to “receiving a trigger” to “performing measurement.” The averaging factor is not cleared; it is incremented. |
|
On |
The instrument repeats a cycle of “waiting for a trigger” to “receiving a trigger” to “performing measurement.” The averaging factor is cleared before the start of measurement after receiving the first trigger. |
The setting made with this command is common to all of the measurement modes (PN, PS, SP, FP, AM, BB and TR). You cannot use a different setting for each measurement mode.
When the averaging mode (set with the :SENS:xx:AVER:STAT command) is off, the averaging trigger mode is not available.