Data Types for Data Transfer

Other topics about Reading-Writing Measurement Data

Overview

This section describes the data types that the E5052B uses for data transfer.

Array Type

If you use any of the following commands, the data transfer will be executed using array-type data. Here, you can choose from among ASCII transfer format, IEEE 64-bit floating point binary transfer format, and IEEE 32-bit floating point binary transfer format.

For phase noise measurement

For spectrum measurement

For frequency/power measurement

For transient measurement

For AM noise measurement

For baseband noise measurement

For user measurement

For segment phase noise measurement

For sending and receiving data to/from VBA program

Block Type

If you use any of the following commands, the data transfer will be executed using block-type data. Here, you can choose either IEEE 64-bit floating point binary transfer format or IEEE 32-bit floating point binary transfer format.