Used to enter numeric data into the E5052B. Press a hardkey or softkey to enter data, and the data entry bar will appear at the top of the screen. To assign a title to a measurement window, the entry bar also allows you to enter letters and symbols by using the front panel keys or mouse.
Data Entry Bar

To manipulate the data entry bar with the front panel keys, it has to be selected as the object to manipulate (focus placed on it). When the focus is placed on the data entry bar, the entire bar is displayed in blue. Pressing or clicking on Focus Key in ENTRY Block enables you to move the focus to the desired object.
Displays the name of the parameter for which data will be entered.
When the data entry bar is displayed for the first time, the current settings are displayed on it. You can change numeric values by typing from the keyboard or in the ENTRY block on the front panel.
Increases or decreases the numeric value in the data entry area in small steps. Use the mouse to manipulate this button.
Increases or decreases the numeric value in the data entry area in large steps. Use the mouse to manipulate this button.
Closes the data entry area (turns off the display). Use mouse to manipulate this button.