Other topics about Setting Control Functions
You can select the display mode of the LCD display from two options: normal display (background: black) and inverted display (background: white). In normal display, the colors of items are preset so that you can recognize them easily on the display of the instrument. On the other hand, in inverted display, items are preset to colors obtained by almost completely inverting the default settings of the normal display; this mode allows
you to use data easily when storing it into a graphic file.
The selection procedure is as follows:
Press Display key.
Click Color Type. Normal indicates normal display and Invert indicates Invert display.
You can set the display color to the normal display or to the inverted display separately for
each of the following items:
Data/memory trace
Labels and lines of graphs
File display of the limit test and limit lines
Background
Set the color of each item by specifying the amounts of red (R), green (G), and blue (B)contained in the color. You can specify each level of R, G, and B in 256 steps (0 to 255). Therefore, 16.77 million colors in total are available by combining the color levels. The table below shows the R, G, and B values for the main colors as a reference.
|
Color |
R |
G |
B |
|
White |
255 |
255 |
255 |
|
Red |
255 |
0 |
0 |
|
Cyan |
0 |
255 |
255 |
|
Gray |
128 |
128 |
128 |
|
Yellow |
255 |
255 |
0 |
|
Blue |
0 |
0 |
255 |
|
Black |
0 |
0 |
0 |
|
Green |
0 |
255 |
0 |
|
Magenta |
255 |
0 |
255 |
The selection procedure is as follows:
Press System > Misc Setup > Display Setup > Color Setup.
Click Normal (for normal display) or Invert (for invert display).
Press the softkey corresponding to the item for which you want to set the display color.
|
SoftKey |
Function |
|
Data Trace (1-8) |
Specifies the data trace of traces 1 to 8 |
|
Memory Trace (1-8) |
Specifies the memory trace of traces 1 to 8 |
|
Graticule Main |
Specifies the graticule label and the outer lines of graphs |
|
Graticule Sub |
Specifies the grid lines of graphs |
|
Limit Fail |
Specifies the fail display in the limit test result |
|
Limit Line |
Specifies the limit line |
|
Background |
Specifies the background |
Click Red and select the amount of red (R) from 0 to 255.
Click Green and select the amount of green (G) from 0 to 255.
Click Blue and select the amount of blue (B) from 0 to 255.
You can reset the display colors in normal display and inverted display to the values of the preset factory state.
The selection procedure is as follows.
Press System > Misc Setup > Display Setup > Color Setup.
Click Normal (for normal display) or Invert (for inverted display).
Click Reset Color > OK.