The E5052B can be connected to external input/output devices such as printer, monitor, keyboard and mouse using any of the serial or USB ports provided in the rear or the front panel.
Other topics about Using Windows
A printer can be connected to the E5052B using the Universal Serial Bus (USB) ports provided in the front or rear panel. The printer driver should be installed by following the instruction of your printer.
A mouse can be connected to the E5052B through the Universal Serial Bus (USB) ports provided in the front or rear panel.
A monitor can be connected to the E5052B using the External Monitor Output Terminal (Video) located in the rear panel of the E5052B.
A keyboard can be connected to the E5052B through the Universal Serial Bus (USB) ports provided in the front or rear panel.