Saving Data

Other topics about Storing Data and Setting

Saving in .csv format

The trace data can be saved in .csv format.

  1. Select the trace which you want to get the data.

  2. Click File in the tool bar.

  3. Select Save Active Trace Data or Save All Trace Data from menu, then the Save Trace As dialog is displayed.

  4. Type desired file name.

  5. Click Save.

Example of File

# Channel 1

# Trace 4

Frequency  Formatted Data  Formatted Data

8.49E+06 -5.84E-02 0.00E+00

1.70E+07 -8.27E-02 0.00E+00

2.55E+07 -1.04E-01 0.00E+00

3.40E+07 -1.32E-01 0.00E+00

4.25E+07 -1.52E-01 0.00E+00

5.09E+07 -1.84E-01 0.00E+00

5.94E+07 -2.18E-01 0.00E+00

6.79E+07 -2.70E-01 0.00E+00

.

(data is continued until the end)

.

Saving in the other format

The trace data can be saved in .csv format.

  1. Click File in the tool bar.

  2. Select Save Data As, then the Save Trace As dialog is displayed.

  3. Select Save As Type.

  4. Type desired file name.

  5. Click Save.

See Save Other Format Topic for more detail