Noise that modulates the phase of the carrier is referred to as amplitude modulation of the carrier. The following procedure describes how to measure AM Noise.
Set up a Phase Noise measurement as described in Setting Up a Phase Measurement.
On the analyzer front panel, press Meas > Main> AM
To create a new AM Noise trace, press Meas
> Main> Other....
The Measure dialog is displayed:

In the Measure dialog, check AM.
In the Measure dialog, check New Trace then select the desired Channel and Window.
The following example displays an AM measurement at
the b4 analyzer input:

The FM/AM column displays the percentage of modulation of the carrier.