How to select and configure Measurement Parameters |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
PN - Integrated phase noise measured AM - Amplitude modulation measured. This parameter measures the percentage of the modulation of the carrier. PM+AM - Sum of Integrated phase noise and Amplitude modulation L(f) - Single sideband phase noise (same as PN), dBc/Hz Sphi(f) - Spectral density of phase fluctuation, dB/Hz Sv(f) - Square root of Spectral density of frequency fluctuations, Hz/sqrt(Hz) Sy(f) - Square root of Spectral density of fractional frequency fluctuations, 1/sqrt(Hz) AVAR - Allan Variance ADEV - Allan Deviation Note: The input receiver number can be changed using the RF Path tab
New Trace - Add a new trace. Channel N - Select a channel number for the new modulation distortion trace. Window N - Select to create the new trace in an existing window or new window. Select All - Select all measurement parameters.
Measured Side Band of Offset> 30 MHz in AM+PMIn PM+AM composite measurement, SSA-X measures Lower Side Band (LSB) and Upper Side Band (USB) for Offset > 30 MHz. The following table shows which side band is measured. The selected Side Band (LSB or USB) is dumped by csv file save (Save/Recall > Save Other > Save Data..., then select file type: trace and phase noise parameter)
The E5055A measures USB for all carrier frequency |
|||||||||||||||
Quick Trace shows an interim result during cross correlation. When the cross correlation factor is a large number, the calculation takes long time. This allows you to notice an incorrect setup earlier.
When the Quick Trace is set at Off (default is Off). The traces are updated only after cross correlation calculation is finished. Quick trace may show strange result for an instant if you measure a noisy signal.