Configure VCO Characterization settings |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Always use Internal Reference - Always use the internal reference despite of the global reference setting. RF 1/2 Input - Select RF input port for 2 port model. Auto range - Check: Attenuator is set automatically by referring the measured carrier power. / Uncheck: Attenuator is set according to Auto setting in the Receiver Attenuator Setting dialog box. Maximum Input Level - Specify the Maximum input level. [...] - Open the following Receiver Attenuator Setting dialog box.
Enable Attenuator Setting - Uncheck: Appropriate attenuator value is set automatically according to the specified Maximum Input Level. / Check: Set the specified attenuator value. Attenuator - This attenuator values is set when Enable Attenuator Setting is checked. |