Specifies settings for embedding and de-embedding Single-Ended (2-port) fixturing circuits.
CALCulate:FSIMulator:SENDed: |
Click on a keyword to view the command details.
See Also
Example Programs
Note: CALC:FSIM commands affect ALL measurements on the specified channel.
CALCulate<cnum>:FSIMulator:SENDed:OORDer <a,b,c,d>
Applicable Models: All (Read-Write) Sets and returns the order in which Single-ended Fixture Operations occur. Learn more about these operations. Note: The operation for ground loop embedding and ground loop de-embedding will always occur as the 3rd step. It cannot be moved. By default, this is after the 2-Port DeEmbedding operation. Note: This command affects ALL measurements on the specified channel. |
|
Parameters |
|
<cnum> |
Channel number of the measurement. There must be a selected measurement on that channel. If unspecified, <cnum> is set to 1. |
<a,b,c,d> |
Order of operations, where: 0 - Port Extension operation 1 - 2-Port DeEmbedding operation 2 - Port Matching operation 3 - Arbitrary Impedance operation |
Examples |
CALC:FSIM:SEND:OORD
1,2,3,0 |
Query Syntax |
CALCulate<cnum>:FSIMulator:SENDed:OORDer? |
Return Type |
Comma-separated values |
0,1,2,3 |
|