Controls writing and reading VNA measurement data.
CALCulate:MEASure: | BUFFer? | X | Y | FDATa | FMEMory | RAW | CATalog? | SDATa | SMEMory | SNP? | PORTs? | SAVE | X | AXIS | DOMain | FIXed | VALue
|
Click a keyword to view the command details.
See Also
See CALCulate:MEASure:X:VALues for stimulus point data.
(Read) CALCulate<cnum>:MEASure<mnum>:DATA:<char>?
Applicable Models: All Reads or writes Measurement data, Memory data, or Normalization Divisor data from the Data Access Map location.
Equation Editor Notes:
Note: The Calc:Data SCORR command to read/write error terms is Superseded with SENS:CORR:CSET:DATA. SCORR commands do NOT accommodate greater than 12 error terms. |
||
Parameters |
||
<cnum> |
Channel number of the measurement (optional). |
|
<mnum> |
Measurement number for each measurement. |
|
<char> |
Formatted measurement data to or from Data Access Map location. Display (access point 2). Note: When querying FDATA, data is received in degrees. When setting phase using FDATA, the command expects the data in radians.
|
|
|
Complex measurement data. Writes data to Data Access Map location. Raw Measurement (access point 0). Note: Write access is forbidden on the standard channel if factory calibration is on (applies to ENA/PXI/Streamline, not to PNA); to disable factory calibration use SYST:FCOR:CHAN:COUP:STAT OFF command.
Reads data from Apply Error Terms (access point 1).
|
|
|
Formatted memory data to or from Data Access Map location. Memory result (access point 4).
|
|
|
Complex memory data to or from Data Access Map location. Memory (access point 3).
|
|
Examples |
CALC:MEAS:DATA:FDATA Data(x) See another example using this command. |
|
Return Type |
|
|
Default |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Read-only) Retrieves frequency tone data from the modulation distortion measurement. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bufferName> |
(string) – Name of the buffer to be read. Note: The following names assume a 2-port VNA. Also, by default, the parameter names assume that VNA Port 1 is connected to the DUT input and VNA Port 2 is connected to the DUT output. If the RF Path settings are changed from the default, the names will change accordingly. For example, if the VNA has 4 ports and Port 4 is connected to the DUT output, the names will change to "PIn1", "POut4", "S11", "S41", etc. Choose from: "POut2" - Power Out "PIn1" - Power In "MSig2" - Modulation Signal Out "MDist2" - Modulation Distortion Out "MGain21" - Modulation Gain "MComp21" - Modulation Compression "PGain21" - Power Gain "S11" - Linear Input Match "S21" - Linear Gain "LPin1" - Linear Power In "LPOut1" - Linear Reflected Power In "LPOut2" - Linear Power Out |
Examples |
CALC:MEAS1:DATA:BUFF:X? "POut2" |
Return Type |
Depends on FORM:DATA command |
Default |
Not Applicable |
Applicable Models: E505xA with VNA ports (Read-only) Retrieves trace data (Y data) from the modulation distortion measurement. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<bufferName> |
(string) – Name of the buffer to be read. Note: The following names assume a 2-port VNA. Also, by default, the parameter names assume that VNA Port 1 is connected to the DUT input and VNA Port 2 is connected to the DUT output. If the RF Path settings are changed from the default, the names will change accordingly. For example, if the VNA has 4 ports and Port 4 is connected to the DUT output, the names will change to "PIn1", "POut4", "S11", "S41", etc. Choose from: "POut2" - Power Out "PIn1" - Power In "MSig2" - Modulation Signal Out "MDist2" - Modulation Distortion Out "MGain21" - Modulation Gain "MComp21" - Modulation Compression "PGain21" - Power Gain "S11" - Linear Input Match "S21" - Linear Gain "LPin1" - Linear Power In "LPOut1" - Linear Reflected Power In "LPOut2" - Linear Power Out |
Examples |
CALC:MEAS1:DATA:BUFF:Y? "POut2" |
Return Type |
Depends on FORM:DATA command |
Default |
Not Applicable |
Applicable Models: E505xA with VNA ports (Write-Read) Sets the raw data for the specified raw parameter buffer. For unratioed parameters, the source port separator can be either ‘,’ or ‘_’. This command applies to a Standard channel only. Application channels will return an error. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
String - (Not case-sensitive) Raw parameter buffer. For example, "S11". |
<dataBlock> |
String - (Not case-sensitive) Raw measurement data. |
Examples |
CALC:MEAS:DATA:RAW "S11",5.85E-002,-7.0E-002,+9.80E-003,+5.40E-002,+2.26E-002,+6.25E-002,-3.47E-002,+4.00E-002 calculate:measure:data:raw "S11",5.85E-002,-7.0E-002,+9.80E-003,+5.40E-002,+2.26E-002,+6.25E-002,-3.47E-002,+4.00E-002 |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:DATA:RAW? "<string>" |
Return Type |
|
Default |
Not Applicable |
Applicable Models: E505xA with VNA ports (Read-only) Returns the list of raw parameters associated with the measurement <mnum>. These are the raw parameters that are actually used by the error correction; the <mnum> measurement may not strictly depend on all of those. For example, 2 port S-parameters. If the DUT has transmission, then changing raw S11 will modify the corrected S22. If transmission is negligible, S22 is unaffected. The list is returned as strings comma separated. For unratioed parameters, the source port separator is ‘_’ instead of ‘,’ to avoid confusion in tokenization. This command applies to a Standard channel only. Application channels will return an error. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Example |
CALC:MEAS1:DATA:RAW:CAT? |
Return Type |
String |
Default |
Not Applicable |
Applicable Models: E505xA with VNA ports (Read-only) Reads SnP data from the selected measurement. Learn more about SnP data. This command is valid ONLY with standard S-parameter measurements.
|
||
Parameters |
||
<cnum> |
Channel number of the measurement (optional). |
|
<mnum> |
Measurement number for each measurement. |
|
<n> |
Amount of data to return. If unspecified, <n> is set to 2. The number you specify must be less than or equal to the number of available ports on the VNA. Choose from: 1 (S1P) returns 1-Port data for the active measurement if the active measurement is a reflection parameter such as S11 or S22. The behavior is UNDEFINED if the active measurement is a transmission parameter such as an S21. 2 (S2P) returns data for the four 2 port parameters associated with the current measurement. Default. Data that is not available is zero-filled. 3 (S3P) returns data for the nine 3 port parameters associated with the current measurement. Data that is not available is zero-filled. 4 (S4P) returns data for the sixteen 4 port parameters associated with the current measurement. Data that is not available is zero-filled. SnP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. See also MMEM:STOR <file>.<snp> |
|
Examples |
CALC:MEAS1:DATA:SNP? 1 |
|
Return Type |
Depends on FORMat:DATA. |
|
Default |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Read-only) Reads SNP data from the selected measurement for the specified ports. Learn more about SNP data. This command is valid ONLY with standard S-parameter measurements.
|
||
Parameters |
||
<cnum> |
Channel number of the measurement (optional). |
|
<mnum> |
Measurement number for each measurement. |
|
<"x,y,z"> |
Comma or space delimited port numbers for which data is requested, enclosed in quotes. SNP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. |
|
Examples |
CALC:MEAS2:DATA:SNP:PORTs? "1,2,4,5,7" 'read data for these ports |
|
Return Type |
Depends on FORMat:DATA |
|
Default |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write-only) Saves SNP data from the selected measurement for the specified ports. Learn more about SNP data.
|
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<"x,y,z"> |
String Comma or space delimited port numbers for which data is requested, enclosed in quotes. |
<filename> |
String Path, filename, and suffix of location to store the SNP data, enclosed in quotes. The suffix is not checked for accuracy. If saving 2 ports, specify "filename.s2p"; If saving 4 ports, specify "filename.s4p.", and so forth. SNP data can be output using several data formatting options. See MMEM:STORe:TRACe:FORMat:SNP. |
[, FAST] |
Reduce the saving time :SENS:CORR:CACH:MODE
should be set at ON. The active measurement must be a corrected S Parameter defined by the port list for the SNP requests. EG: "S33" is not a proper selected measurement with CALC:DATA:SNP:PORTS? <1,2> |
Examples |
CALC:MEAS2:DATA:SNP:PORTs:Save '1,2,4','D:\MyData.s3p';*OPC? |
Return Type |
Depends on FORMat:DATA |
Default |
Not Applicable |
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA, M983xA (Write-Read) Sets the X-axis of the selected measurement to a DC Source. This command does not change the default setting for new traces. |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
String - (Not case-sensitive) For all channels EXCEPT DIQ, choose from the following: "Default" - The default X-axis setting for the selected measurement. For Application measurements, the X-Axis domain is set with specific commands. "AO1" - Internal DC source #1 "AO2" - Internal DC source #2 Note: For DIQ channels, see CALC:MEAS:X:AXIS:DOMain
For Modulation Distortion Channels (MOD), choose from: "SA Frequency" - SA display showing the SA frequency settings. "Power In" - Displays input power sweep. "Power Out" - Displays output power sweep. "Measured Carrin" - Measured input band power. "Measured CarrOut" - Measured output band power.
For Modulation Distortion Converters Channels (MODX), choose from: "SA Freq In" - SA display showing mixer input range. "SA Freq Out" - SA display showing mixer output range. "Power In" - Displays input power sweep. "Power Out" - Displays output power sweep. "Measured Carrin" - Measured input band power. "Measured CarrOut" - Measured output band power.
|
Examples |
CALC:MEAS:DATA:X:AXIS 'Default' calculate:measure:data:x:axis "AO1" |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:DATA:X:AXIS? |
Return Type |
String |
Default |
"Default" |
Applicable Models: N522xB, N523xB, N524xB, M983xA (Write-Read) Sets and returns the X-Axis domain of the selected DIQ measurement. |
|||||||||||||
Parameters |
|
||||||||||||
<cnum> |
Channel number of the measurement (optional). |
||||||||||||
<mnum> |
Measurement number for each measurement. |
||||||||||||
|
|
||||||||||||
Example |
1. CALC:MEAS:DATA:X:AXIS:DOM "Power" 2. CALC:MEAS:DATA:X:AXIS "Port 1" |
||||||||||||
Query Syntax |
CALCulate<ch>:MEASure<mnum>:DATA:X:AXIS:DOMain? |
||||||||||||
Return Type |
String |
||||||||||||
Default |
CALC:MEAS:DATA:X:AXIS:DOMain: "Frequency" CALC:MEAS:DATA:X:AXIS: "F1" |
||||||||||||
Applicable Models: N524xB models with Option S93070xB (Write-Read) Sets the X-axis fixed parameter for a power sweep measurement in a Modulation Distortion channel. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<string> |
String - (Not case-sensitive) For Modulation Distortion Channels (MOD), choose from: "SA Frequency" - SA display showing the SA frequency settings.
For Modulation Distortion Converters Channels (MODX), choose from: "SA Freq In" - SA display showing mixer input range. "SA Freq Out" - SA display showing mixer output range.
|
Examples |
CALC:MEAS2:DATA:X:AXIS:FIX:PAR "SA Frequency" calculate:measure2:data:x:axis:fixed:parameter "SA Freq In" |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:DATA:X:AXIS:FIXed:PARameter? |
Return Type |
String |
Default |
"SA Frequency" |
Applicable Models: N524xB models with Option S93070xB (Write-Read) Sets the X-axis fixed parameter spectrum analyzer frequency value for a power sweep measurement in a Modulation Distortion channel. |
|
Parameters |
|
<ch> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
<num> |
Fixed parameter value. |
Examples |
CALC:MEAS2:DATA:X:AXIS:FIX:PAR:VAL 1.5e9 calculate:measure2:data:x:axis:fixed:parameter:value 1.5e9 |
Query Syntax |
CALCulate<ch>:MEASure<mnum>:DATA:X:AXIS:FIXed:PARameter:VALue? |
Return Type |
Numeric |
Default |
Not Applicable |
Applicable Models: N522xB, N523xB, N524xB, M937xA, P937xA (Read-only) Returns the stimulus values for the selected measurement in the current units. You can select one measurement for each channel using Calc:Par:MNUM or Calc:Par:Select. Learn more. This command can be used for all Measurement Classes. Note: To avoid frequency rounding errors, specify FORM:DATA <Real,64> or <ASCii, 0> |
|
Parameters |
|
<cnum> |
Channel number of the measurement (optional). |
<mnum> |
Measurement number for each measurement. |
Examples |
1.
Calc:Par:Sel "MyGCATrace" |
Return Type |
Depends on FORM:DATA command |
Default |
Not applicable |