Specifies the settings to remotely control the rear panel connectors, an external test set, Calpod modules, and ECal Module state.
CONTrol DC | INPut | CURRent? | OUTPut | VOLTage ECAL:MODule: | PATH: | COUNt? | STATe | STATe PHASe | COUNt? | MODule | DATA | STORe | MODel? | SERial? | SETup | AIO | PIN | COUNt? | FUNCtion | CATalog? | CHANnel |
Click on a keyword to view the command details.
Blue command is superseded.
See Also
Material Handler IO connector
Applicable Models: E505xA (Write-Read) Sends commands that control a Calpod module. Reads query versions Calpod commands. See ALL Calpod commands. |
|
Parameters |
|
<string> |
Calpod command. See ALL Calpod commands that can be used in this string. |
Write Example |
CONT:CALP:COMM 'CALP:INIT:ACT' 'Enclose all strings in SINGLE quotes (NOT double quotes) |
Query Syntax |
CONTrol:CALPod:COMMand? <string> Relevant only for query strings. |
Read Example |
CONT:CALP:COMM? '*OPC?' 'returns 0 if the calpod software is currently processing an operation 'returns 1 if operations are complete |
Return Type |
String |
Not Applicable |
|
Applicable Models: E505xA (Read) Return the current measurement for DC sources. |
|
Parameters |
|
<device> |
String. Choose from: VControl VSupply1 VSupply2 |
Examples |
CONT:DC:INP:CURR? "VControl" control:dc:input:current? "vsupply2" |
Query Syntax |
CONTrol:DC:INPut:CURRent? <device> |
Return Type |
Numeric |
N/A |
|
Applicable Models: E505xA (Read-Write) Set the voltage immediately. This function is not available on Soft Front Panel. |
|
Parameters |
|
<device> |
String. Choose from: VControl VSupply1 VSupply2 |
<value> |
Voltage value. |
Examples |
CONT:DC:OUTP:VOLT "VControl",2 control:dc:output:voltage "vsupply2",1 |
Query Syntax |
CONTrol:DC:OUTPut:VOLTage? <device> |
Return Type |
Numeric |
0 |
|
Applicable Models: E505xA with VNA ports (Read-only) Returns the number of unique states that exist for the specified path name on the selected ECal module. This command performs exactly the same function as SENS:CORR:CKIT:ECAL:PATH:COUNt? Use the CONT:ECAL:MOD:PATH:STAT command to set the module into one of those states. Use SENS:CORR:CKIT:ECAL:PATH:DATA? to read the data for a state. |
|
Parameters |
|
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
<name> |
Name of the path for which to read number of states. Choose from: Reflection paths
Transmission paths
Note: For each transmission path, the first of the available states is the through state, the second is the confidence (attenuator) state. |
Examples |
CONT:ECAL:MOD:PATH:COUNt? A control:ecal:module2:path:count? cd |
Return Type |
Integer |
Not Applicable |
|
Applicable Models: E505xA with VNA ports (Write-only) Sets the internal state of the selected ECAL module. This command supersedes CONT:ECAL:MOD:STAT.
|
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Parameters |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
[num] |
Optional argument. USB number of the ECal module. If unspecified (only one ECal module is connected to the USB), <num> is set to 1. If two or more modules are connected, use SENS:CORR:CKIT:ECAL:LIST? to determine how many, and SENS:CORR:CKIT:ECAL:INF? to verify their identities. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<path> |
Path name for which to set a state. Note: The impedance paths are not independent. For example, changing the impedance presented on path A will cause a change to the impedance on path B. Choose from: Reflection paths
Transmission paths
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<stateNum> |
Number of the state to set. Refer to the following table to associate the <stateNum> with a state in your ECal module. In addition, CONT:ECAL:MOD:PATH:COUNt? returns the number of states in the specified ECal module.
** The following modules have only FOUR Impedance states (1, 2, 3, 4): N4690B ,N4691B ,N4692A ,N4696B, N7550A - N7556A. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Examples |
CONT:ECAL:MOD:PATH:STATe A,5 control:ecal:module2:state BC,1 |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Query Syntax |
Not Applicable |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Not Applicable |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Applicable Models: E505xA with VNA ports (Read only) Reads the number of phase reference modules connected. |
|
Parameters |
None |
Examples |
CONT:PHAS:COUN? control:phase:count? |
Return Type |
Numeric value |
N/A |
|
Applicable Models: E505xA with VNA ports (Write-only) Reads the calibration data from the phase reference of the specified module (x), and writes the data to the Path |
|
Parameters |
|
<path> |
(String) Directory path to stored data. |
Examples |
CONT:PHAS:MOD1:DATA:STOR "D:MyPhaseRefCalData.csv" control:phase:module1:data:store "D:MyPhaseRefCalData.csv" |
Return Type |
N/A |
N/A |
|
Applicable Models: E505xA with VNA ports (Read only) Reads the model number of the specified module (x). |
|
Parameters |
None |
Examples |
CONT:PHAS:MOD1:MOD? control:phase:module1:model? |
Return Type |
String |
N/A |
|
Applicable Models: E505xA with VNA ports (Read only) Reads the serial number of the specified module (x). |
|
Parameters |
|
Examples |
CONT:PHAS:MOD1:SER? control:phase:module1:serial? |
Return Type |
Numeric |
N/A |
|
Applicable Models: E505xA with VNA ports
(Write-only) Turns on the phase reference, and sets the divide number. |
|
Parameters |
|
<divideNumber> |
Divide number can be 1, 2, 4, 8, 16. |
Examples |
CONT:PHAS:MOD1:SET 2 control:phase:module1:setup 2 |
Return Type |
Numeric |
N/A |
|
Applicable Models: E505xA (Read only) Read the total number of pin on the application I/O. In case for the E505xA, always 15. For more information, see application I/O. |
|
Parameters |
None |
Examples |
CONT:SIGN:AIO:PIN:COUN? control:signal:aio:pin:count? |
Query Syntax |
CONTrol:SIGNal:AIO:PIN:COUNt? |
Return Type |
Numeric value |
15 |
|
Applicable Models: E505xA (Write-Read) Set and Read the function for the specified port in the application I/O interface. The assigned settings are not saved in a state file, but the setting is stored when changing function and recall them at the next firmware start up. |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Parameters |
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<pin> |
Pin Number. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
<func> |
function name
*1) For Noise Figure switch control, the signal is asserted no matter which pins are used in the NF channel if the port index(x) is not specified. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Examples |
CONT:SIGN:AIO:PIN:FUNC "LOW" control:signal:aio5:pin:function "NF_SOURCE15" |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Query Syntax |
CONTrol:SIGNal:AIO:PIN:FUNC? |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Return Type |
<sting> |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
See the table in <func> |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Applicable Models: E505xA (Read Only) Read the list of the available function for the specified pin in the application I/O. Example, "RF_PULSE_MOD_IN" is returned for the pin 8. |
|
Parameters |
|
<pin> |
Pin Number. |
Examples |
CONT:SIGN:AIO:PIN3:FUNC:CAT? control:signal:aio:pin3:function:catalog? |
Query Syntax |
CONTrol:SIGNal:AIO:PIN:FUNC:CAT? |
Return Type |
<sting>, available function list with Comma separated chars |
See the table in <func> of CONTrol:SIGNal:APPLication:FUNC? |
|
Applicable Models: E505xA (Write-Read) Set and read the function for the selected pin on the Application I/O connector. It is set on channel basis and reflected only when “CHANNEL_CTRL” is selected in :CONTrol:SIGNal:AIO:PIN<pin>:FUNCtion <func> for the specified pin. The setting is saved in the state file and subject to preset. Function can be selected from Output signals |
|
Parameters |
|
<pin> |
Pin Number 1-5, 10-13 |
<ch> |
Channel number |
Examples |
:CONT:SIGN:AIO:PIN3:CHAN1:FUNC? :CONT:SIGN:AIO:PIN3:CHAN1:FUNC “HIGH” |
Query Syntax |
CONTrol:SIGNal:AIO:PIN:CHAN:FUNC? |
Return Type |
<char> |
HIGH |
|
Applicable Models: E505xA (Read Only) Read the catalog of the functions assignable to the pin on the Application I/O connector. |
|
Parameters |
|
<pin> |
Pin Number 1-5, 10-13 |
Examples |
:CONT:SIGN:AIO:PIN5:CHAN1:FUNC:CAT? control:signal:aio:pin5:channel:function:catalog? |
Query Syntax |
CONTrol:SIGNal:AIO:PIN:CHAN:FUNC:CAT? |
Return Type |
Comma separated chars |
NA |
|
Applicable Models: E505xA (Read only) Read the level of the specified INPUT pin of the application I/O. This command reads the level immediately after its execution. It is not necessary to assign the pin as INPUT by command. When the specified pin number is 6 to 9 or 14, "Specified Application IO port is not input port." error is returned. |
|
Parameters |
|
<pin> |
Pin Number. (E5080B: 1 to 5, 10 to 13) |
Examples |
CONT:SIGN:AIO:PIN:INP2:LEV? control:signal:aio:pin:input1:level? |
Query Syntax |
CONTrol:SIGNal:AIO:PIN:INPut:LEVel? |
Return Type |
Char ("HIGH" or "LOW") |
N/A |
|