LXI Command


SCPI Command Tree

LXI:IDENtify[:STATe] <bool>

Applicable Models: N522xB, N523xB, N524xB, E5080A/B

(Read-Write)  Sets and returns the status of the LXI LAN status indicator on the LAN Status dialog.

Parameters

 

<bool>

Choose from:

OFF or 0 - Changes the LXI Status indicator to ‘NORMAL’ and closes the dialog if it was opened by this command.

ON or 1 - Changes the LXI Status indicator to ‘IDENTIFY’ and opens the dialog if it was not already open.

Examples

LXI:IDEN 1
lxi:identify:state off

Query Syntax

LXI:IDENtify[:STATe]?

Return Type

Boolean

Default

OFF