A analyzer is LXI-1.1
compliant if the
logo appears on the dialog box shown
below.
Learn more about LXI at http://www.lxistandard.org/
Learn more about VXI at http://www.vxibug.org/
When a LAN connection is used with the analyzer , the LAN Status dialog allows you to see the IP address and other LAN connection properties.
How to view LAN Status |
|
Using Hardkey/SoftTab/Softkey |
Using Menus |
|
|
Indicator Shows the current status of the LAN connection. NORMAL - Indicates that the analyzer LAN is ready for communication. IDENTIFY - Indicates that a remote computer has invoked an LXI identification operation on the analyzer using the web-based interface or LXIDeviceIDState COM property. FAULT - Indicates that the analyzer LAN interface is not connected to the Internet. IP Address Shows the current IP address of the analyzer . IPv6 Link-Local Address Shows the current IPv6 address of the analyzer . Computer Name Shows the full computer name of the analyzer . Learn how to change this. If you see the IP address listed here, that means there is no DNS server specified in the network setup. MAC Address Shows the unique address of the analyzer computer. Also known as HostID. LAN Reset Provides a LAN Configuration Initialize (LCI) mechanism. Press to return the following settings to factory default conditions:
|
If your analyzer is LXI Class C compliant (see above), you can connect to the analyzer using a web browser over an internet connection.
To do this, when the above dialog indicates a NORMAL condition:
From a web browser, type http://<your_analyzer _computer_name>.
Type the log on User Name and Password
You will see the welcome screen with connection links.