Sense:Clock Command


SENSe:CLOCk:INTernal:ALIGnment

 | AUTO:STATe

 | IMMediate

 


SENSe<cnum>:CLOCk:INTernal:ALIGnment:AUTO:STATe <bool>

Applicable Models: E505xA

(Read-Write) Sets and read the state of automatic clock alignment for all channels. The clock alignment takes time and the auto alignment may disturb your measurement.  If the analyzer get warm up well and your environment temperature is very stable, you may turn this off.

Parameters

 

<cnum>

Channel number. This parameter is ignored.

<bool>

Auto clock alignment state. Choose from:

O or OFF - Do not perform clock alignment automatically. "Align recommended" message is displayed if the alignment is required.  

1 or ON - Clock alignment is automatically performed  as necessary.

Examples

SENS:CLOC:INT:ALIG:AUTO:STAT OFF
sense:clock:internal:alignment:auto:state 0

Query Syntax

:SENSe<cnum>:CLOCk:INTernal:ALIGnment:AUTO:STATe?

Return Type

Boolean

Default

ON or 1


SENSe<cnum>:CLOCk:INTernal:ALIGnment:IMMediate

Applicable Models: E505xA

(Write only) Perform the clock alignment once immediately.

Parameters

 

<cnum>

Channel number. This parameter is ignored.

Examples

SENS:CLOC:INT:ALIG:IMM

Query Syntax

Not applicable

Default

Not applicable