Controls the PXI DC measurement.
SENSe:DC:
| SAMPles | POINts |
Click on a keyword to view the command details.
Applicable Models: E505xA (Read-Write) Sets and reads the DC measurement number of sample counts per one point measurement. |
|
Parameters |
|
<ch> |
Any existing channel number. If unspecified, value is set to 1. |
<name> |
String. DC Meter Name. |
<num> |
Sample count value. Value range: 1 to 100000, step 1 (SMU), |
Examples |
SOUR:DC:SAMP:POINT "SMU1", 1000 |
Query Syntax |
SENSe<ch>:DC:SAMPLes:POINTs? <name> |
Return Type |
Numeric |
|
|