SYSTem:CAPability:HARDware:MODule Commands


Returns various capabilities of the PXIe/USB VNA.

SYSTem:CAPability:HARDware:MODule:

COUNt?

SERial?

MODel?

OPT?

FPGA?

     | COUNt?

Click on a red keyword to view the command details.

See Also


SYSTem:CAPability:HARDware:MODule:COUNt?

Applicable Models: All but M9485A

(Read-only) Returns the number of modules that are part of the current VNA instance. Learn more about Multiport VNA.

Parameters

None

Examples

SYST:CAP:HARD:MOD:COUNt?

Return Type

Numeric

Default

Not Applicable


SYSTem:CAPability:HARDware:MODule<n>:SERial?

Applicable Models: All

(Read-only) Returns the serial number of the specified module.

Parameters

 

<n>

Module number. This is the order in which the module appears in the Multiport VNA. This is not the slot number in a chassis. Learn more about module number.

Examples

SYST:CAP:HARD:MOD3:SERial?

Return Type

String

Default

Not Applicable


SYSTem:CAPability:HARDware:MODule<n>:MODel?

Applicable Models: All

(Read-only) Returns the model number of the specified module. See frequency ranges of VNA models.

Parameters

 

<n>

Module number. This is the order in which the module appears in the Multiport VNA. This is not the slot number in a chassis. Learn more about module number.

Examples

SYST:CAP:HARD:MOD3:MODel?

Return Type

String

Default

Not Applicable


SYSTem:CAPability:HARDware:MODule<n>:OPT?

Applicable Models: All

(Read-only) Returns the options that are installed in the specified module. See a list of VNA options. See SYSTem:CAPability:LICenses:CATalog? for software product/options.

Parameters

 

<n>

Module number. This is the order in which the module appears in the Multiport VNA. This is not the slot number in a chassis. Learn more about module number.

Examples

SYST:CAP:HARD:MOD3:OPT?

'Possible return string: "010,551"

Return Type

A comma-separated string.

Default

Not Applicable


SYSTem:CAPability:HARDware:MODule<n>:FPGA:COUNt?

Applicable Models: All

(Read-only) Returns the number of FPGA boards in the module.

Parameters

 

<n>

Module number. This is the order in which the module appears in the Multiport VNA. Learn more about module number.

Examples

SYST:CAP:HARD:MOD3:FPGA:COUNt?

Return Type

Numeric

Default

Not Applicable


SYSTem:CAPability:HARDware:MODule<n>:FPGA<x>?

Applicable Models: All

(Read-only) Returns the version number of specified FPGA board.

Parameters

 

<n>

Module number. This is the order in which the module appears in the Multiport VNA. Learn more about module number.

<x>

FPGA board number. Choose from 1 to the value returned by SYST:CAP:HARD:MOD<n>:FPGA:COUNt?

Examples

SYST:CAP:HARD:MOD3:FPGA2?

Return Type

String

Default

Not Applicable