These commands control the loading and storing of eye bit pattern and mask files.
MMEMory:TDR LOAD | EYE | BPATtern | MASK | STATe STORe | EYE | BPATtern | MASK | FDATa | ALL | SNP | STATe
|
Click on a red keyword to view the command details.
See Also
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command loads the specified user bit pattern file. The extension of file should be .txt. The bit pattern editing is not available through the command. |
|
Parameters |
|
<filename> |
File name of the user bit pattern (.txt) |
Examples |
MMEM:TDR:LOAD:EYE:BPAT
"C:\TDR\mybitpattern.txt" |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command loads eye-mask file. The format of the eye mask file should be the same as the format of the Infiniium DCA (86100C). The extension of the file should be .msk. The MASK pattern editing is not available through the command. |
|
Parameters |
|
<filename> |
File name of the eye mask (.msk) |
Examples |
MMEM:TDR:LOAD:EYE:MASK
"C:\TDR\FC0133.msk" |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) Loads the specified instrument state file (.sta). |
|
Parameters |
|
<filename> |
String - Name of any valid file that does not already exist. |
Examples |
MMEM:TDR:LOAD:STAT 'myState' mmemory:tdr:load:state 'c:\tdr\myState.sta' |
Query Syntax |
Not applicable |
Default |
Not applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command stores the user bit pattern file. The extension of file should be .txt. The bit pattern editing is not available through the command. |
|
Parameters |
|
<filename> |
File name of the user bit pattern (.txt) |
Examples |
MMEM:TDR:STOR:EYE:BPAT
"C:\TDR\mybitpattern.txt" |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) This command stores the eye-mask file. The format of the eye mask file should be the same as the format of the Infiniium DCA (86100C). The extension of the file should be .msk. The MASK pattern editing is not available through the command. |
|
Parameters |
|
<filename> |
File name of the eye mask (.msk) |
Examples |
MMEM:TDR:STOR:EYE:MASK
"C:\TDR\mymask.msk" |
Default |
Not Applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) Stores the specified measurement data file of the active trace. |
|
Parameters |
|
<filename> |
String - Name of any valid file that does not already exist. |
Examples |
MMEM:TDR:STOR:FDAT 'myFdata' mmemory:tdr:store:fdata 'c:\tdr\myFdata' |
Query Syntax |
Not applicable |
Default |
Not applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) Stores the specified measurement data file for all traces. |
|
Parameters |
|
<filename> |
String - Name of any valid file that does not already exist. |
Examples |
MMEM:TDR:STOR:FDAT:ALL 'myFdata' mmemory:tdr:store:fdata:all 'c:\tdr\myFdata' |
Query Syntax |
Not applicable |
Default |
Not applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) Stores the SnP measurement data. Learn more about SnP data. |
|
Parameters |
|
<n> |
SnP measurement data to store. If unspecified, <n> is set to 2. The number you specify must be less than or equal to the number of available ports on the VNA. Choose from: 1 (S1P) stores 1-Port data for the active measurement if the active measurement is a reflection parameter such as S11 or S22. The behavior is UNDEFINED if the active measurement is a transmission parameter such as an S21. 2 (S2P) stores data for the four 2 port parameters associated with the current measurement. Default. Data that is not available is zero-filled. 3 (S3P) stores data for the nine 3 port parameters associated with the current measurement. Data that is not available is zero-filled. 4 (S4P) stores data for the sixteen 4 port parameters associated with the current measurement. Data that is not available is zero-filled. |
Examples |
MMEM:TDR:STOR:SNP 1 mmemory:tdr:store:snp 1 |
Query Syntax |
Not applicable |
Default |
Not applicable |
Applicable Models: All with TDR Options (S9x011A/B) (Write-only) Stores the specified instrument state file (.sta). |
|
Parameters |
|
<filename> |
String - Name of any valid file that does not already exist. |
Examples |
MMEM:TDR:STOR:STAT 'myState' mmemory:tdr:store:state 'c:\tdr\myState.sta' |
Query Syntax |
Not applicable |
Default |
Not applicable |