The software option can be installed by yourself. See https://www.keysight.com/find/LicensingSupport about detailed Keysight license information.
Visit http://www.keysight.com/find/softwaremanager
Log in or register your name if first time log-in.
Click “You can add a new certificate”
Locate the Software License Entitlement Certificate.
Enter your “Order Number” and “Certificate Number” on Software Entitlement Certificate.
Follow the instructions to register the ordered software licenses.
Click “You can request new licenses”
Select your required license (ex. S9xxxxxx)
Add your HOST ID.
Node-locked
/ Transportable / Trial Licenses
The license file can be copied to the root directory of the USB memory
device and then connected to the analyzer. The Keysight License Manager
is always running, and it scans the root directory of any new drive
looking for license files. When the file is found, the licenses are
automatically installed, and a notification is displayed on the screen.
If the licenses are not installed automatically, then the following
instructions should be followed.

or

Floating
License
USB Portable
License
Click “Assign License” at the bottom.
Follow the instructions.
The message with license file (.lic) is sent to your email address.
Note: Do not install the floating/USB licenses on Keyight License Manager. Use Keysight License Manager 6 instead.
Execute the Keysight License Manager from Start Menu in Windows
Click the wrench icon on the right upper of the dialog box.
Select Install License File...
Detailed instructions can also be found in the Keysight License Manager help.
The floating license allows you to borrow/return the license from the license server. Your local controller can be a license server if required.
Make sure if the license has already been installed in the license server.
Execute the Keysight License Manager 6 as Administrator from Start Menu in Windows on the analyzer or controller for analyzer.
Click Specify a remote floating license server, then enter the host name or IP address of the license server.
Select Borrow License Tab, then click Borrow a floating license.
Select the required license and specify the return date.
Select View License Tab, then confirm if the selected license is installed.
Detailed instructions can also be found in the Keysight Licensing Administrator's Guide
https://literature.cdn.keysight.com/litweb/pdf/5951-5739.pdf
Download a Keysight License Manager 6 from https://www.keysight.com/find/LicensingSupport and install it on a PC which you will assign as a license server. If you want to use your controller as a server, the installation is not necessary. See next.
Execute the Keysight License Manager 6 as Administrator from Start Menu in Windows.
Click Add/remove a license on your local machine.
Select Add license to the floating license serve to be used by other machines.
Click Browse… to select license file (.lic), then click Next.
Select View License Tab, then confirm if the selected license is installed.
The network connection is not required when your controller is used as a license server.
Execute the Keysight License Manager 6 as Administrator from Start Menu in Windows on the analyzer or controller for analyzer.
Click Add/remove a license on your local machine.
Select Select a product to license and use on the machine.
Select ENA for SSA-X.
lick Browse… to select license file (.lic), then click Next.
Select View License Tab, then confirm if the selected license is installed.
When the VNA does not detect the floating license, execute the following procedure.
Execute C:\WIndows\system32\services.msc
and find EEsof EDA License Server.
If the status is either blank (Stopped) or status type is Automatic (Delayed Start), then right click and select Properties.
Change the status type from Automatic (Delayed Start) to Automatic,
then click Start of the Service
Status.

Confirm if the Status is changed to Started
and Automatic.

The application/option is enabled only when the analyzer or controller has both license and the corresponding USB dongle. A license file can be installed on many analyzers or controllers. The application is activated while the dongle is plugged in.
Execute the Keysight License Manager 6 as Administrator from Start Menu in Windows on the analyzer or controller for analyzer.
Click Add/remove a license on your local machine.
Select Select a product to license and use on the machine.
Select ENA for SSA-X.
Click Browse… to select license file (.lic), then click Next.
Select View License Tab, then confirm if the selected license is installed.
When you use the application on the analyzer, connect the dongle in the USB port to enable the capability for license.
Note: If your analyzer or controller does not detect the dongle, download and install the FLEXID10USBDongle Driver package for your platform from https://www.keysight.com/find/LicensingUsbDriver.
Detailed instructions can also be found in the Keysight Licensing Administrator's Guide.
https://literature.cdn.keysight.com/litweb/pdf/5951-5739.pdf
The HOST ID will be asked when you get the license file.
HOST ID is shown in the Keysight License Manager. Keyight License Manager can be executed from Start Menu in Windows.
The HOST ID syntax is {Model No.},{Serial Number}, ex: E5055A,MY12345678
HOST ID is Mac address
On the server machine,execute getmac /v /fo list. Your host ID is listed as the Physical Address of the Network Adapter.
HOST ID is printed on a USB dongle.
The USB dongle can be ordered as an option of USB portable licence or Keysight P/N E8900-80036 Hardware Key-USB Port FLEX10.