Improving Measurement Throughput

This section explains the methods to improve measurement throughput.

Other topics about Optimizing Measurements

Turning OFF the updating of information displayed on the LCD screen

Turning OFF the updating information feature displayed on the LCD screen eliminates the processing time required to update displays within the analyzer, hence improves the measurement throughput. If it is not necessary to check displayed information during measurements, turning OFF real-time updating is an effective means of improving throughput.

The updating of information displayed on the LCD screen can be switched using the following procedure:

Turning OFF the updating of information

  1. Press Display.

  2. Click Update to switch the updating of displayed information on the LCD screen ON/OFF.

When the LCD screen update is turned OFF, Update Off appears on Instrument Status Bar.