Updating Firmware

Other topics about Maintenance

Overview

User can update E5061B firmware by themselves. The latest firmware can be downloaded from the http://www.keysight.com/find/ena_support.

Updating firmware does not include the following software update.

Procedure

Firmware Revision A.02.xx

  1. Press System > Service Menu > Exit to terminate the E5061B application.

  2. Download the latest firmware from the download site. (E5061.exe). f you use your local PC to download,  save the file to a USB mass storage device in order to move it to E5061B, then connect the USB mass storage device into the front USB port of the E5061B.

  3. Double click E5061.exe to install the firmware.

  4. Follow the instruction of windows installer. After the installation is finished, the instrument restarts.

  5. Press System > Firmware Revision to confirm the firmware revision you have just installed.

Firmware Revision A.01.xx  

  1. Download the latest firmware from the download site. It is prepared as execution file (E5061B_xx.xx.exe).

  2. Run the E5061B_xx.xx.exe to extract the E5061B.msi.

    If you use your local PC to download,  save the file to a USB mass storage device in order to move it to E5061B, then connect the USB mass storage device into the front USB port of the E5061B.

  3. Press System > Service Menu > Update Firmware. Then, the password dialog box appears.

  4. Type e506xa as the password, then click OK.

  5. In Open dialog box, select E5061.msi, then press Open. Then the windows installer appears.

  6. Follow the instruction of windows installer.

  7. After the installation is finished, the instrument restarts.

  8. Press System > Firmware Revision to confirm the firmware revision you have just installed.