SCPI.CALCulate(Ch).PARameter(Tr).SELect

Object type

Method (Write only)

Syntax

SCPI.CALCulate(Ch).PARameter(Tr).SELect

Description

This command sets the selected trace (Tr) of selected channel (Ch) to the active trace.

You can set a trace to be displayed only to the active trace. If this object is used to set a trace displayed to the non-active trace, an error occurs during execution and the object is ignored. (No read)

Variable

None

Examples

SCPI.CALCulate(2).PARameter(2).SELect

Related objects

SCPI.CALCulate(Ch).SELected.CORRection.EDELay.TIME

SCPI.DISPlay.WINDow(Ch).ACTivate

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.DCOFfset

Equivalent key

Trace Prev

Trace Next

Equivalent SCPI command

Syntax

:CALCulate{[1]-4}:PARameter{[1]-4}:SELect

Example of use

10 OUTPUT 717;":CALC2:PAR2:SEL"