SCPI.SENSe(Ch).CORRection.EXTension.AUTO.DCOFfset

Object type

Property (Read-Write)

Syntax

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.DCOFfset = Status

Status = SCPI.SENSe(Ch).CORRection.EXTension.AUTO.DCOFfset

Description

This command enables/disables or gets the usage of DC Offset value for the results of the auto port extension, for the selected channel (Ch).

Variable

Parameter

Status

Description

ON/OFF the usage of DC Offset value for the results of the auto port extension

Data type

Boolean type (Boolean)

Range

Select from either of the following:

  • True or ON: Uses the DC Offset value for the results.

  • False or OFF: Does not use the DC Offset value for the results.

Preset value

False or OFF

Examples

Dim Dcof As Boolean
SCPI.SENSe(1).CORRection.EXTension.AUTO.DCOFfset = True
Dcof = SCPI.SENSe(1).CORRection.EXTension.AUTO.DCOFfset

Related objects

SCPI.CALCulate(Ch).PARameter(Tr).SELect

SCPI.CALCulate(Ch).SELected.CONVersion.FUNCtion

SCPI.SENSe(Ch).CORRection.EXTension.STATe

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.CONFig

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.LOSS

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.MEASure

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.PORT(Pt)

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.RESet

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.STARt

SCPI.SENSe(Ch).CORRection.EXTension.AUTO.STOP

Equivalent key

Cal > Port Extensions > Auto Port Extension > Adjust Mismatch

Equivalent SCPI command

Syntax

:SENSe{[1]-4}:CORRection:EXTension:AUTO:DCOFfset {ON|OFF|1|0}

:SENSe{[1]-4}:CORRection:EXTension:AUTO:DCOFfset?

Query response

{1|0}<newline><^END>

Example of use

10 OUTPUT 717;":SENS1:CORR:EXT:AUTO:DCOF ON"
20 OUTPUT 717;":SENS1:CORR:EXT:AUTO:DCOF?"
30 ENTER 717;A