Property (Read-Write)
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.MARKer = Status
Status = SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.MARKer
This command turns ON/OFF the marker display of the bandwidth test, for the active trace of selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
Parameter |
Status |
Description |
ON/OFF of the bandwidth marker. |
Data type |
Boolean type (Boolean) |
Range |
Select from the following.
|
Preset value |
False or OFF |
Dim BLimMk As Boolean
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.BLIMit.DISPlay.MARKer = True
BLimMk = SCPI.CALCulate(1).SELected.BLIMit.DISPlay.MARKer
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.BLIMit.STATe
SCPI.CALCulate(Ch).SELected.BLIMit.DISPlay.VALue
Analysis > Bandwidth Limit > BW Marker
:CALCulate{[1]-4}[:SELected]:BLIMit:DISPlay:MARKer {ON|OFF|1|0}
:CALCulate{[1]-4}[:SELected]:BLIMit:DISPlay:MARKer?
{1|0}<newline><^END>
10 OUTPUT 717;":CALC1:BLIM:DISP:MARK ON"
20 OUTPUT 717;":CALC1:BLIM:DISP:MARK?"
30 ENTER 717;A