Property (Read Only)
Status = SCPI.CALCulate(Ch).SELected.BLIMit.FAIL
This command gets the bandwidth limit test results, for the active trace of the selected channel (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command).
|
Parameter |
Status |
|
Description |
The bandwidth limit test result |
|
Data type |
Long integer type (Long) |
|
Range |
Returns from the following.
|
|
Note |
When the bandwidth limit test is set to OFF, the 0 is always read out. |
Dim Result As Integer
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.BLIMit.STATe = 1
Result = SCPI.CALCulate(1).SELected.BLIMit.FAIL
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.BLIMit.STATe
No equivalent key is available on the front panel.
:CALCulate{[1]-4}[:SELected]:BLIMit:FAIL?
{0|1|-1}<newline><^END>
(0: Pass, 1: Fail (Wide), -1:Fail (Narrow), When the bandwidth limit test is set to OFF, 0 is always read out.)
10 OUTPUT 717;":CALC1:BLIM:FAIL?"
20 ENTER 717;A