SCPI.CALCulate(Ch).SELected.FILTer.GATE.TIME.STOP

Object type

Property (Read-Write)

Syntax

SCPI.CALCulate(Ch).SELected.FILTer.GATE.TIME.STOP = Value

Value = SCPI.CALCulate(Ch).SELected.FILTer.GATE.TIME.STOP

Description

This command sets/gets the stop value of the gate used for the gating function of the time domain function, for the active trace of the selected channel (Ch).

Variable

Parameter

Value

Description

The stop value of the gate

Data type

Double precision floating point type (Double)

Range

Varies depending on the frequency span and the number of points.

Preset value

1E-8

Unit

s (second)

Note

If the specified variable is out of the allowable setup range, the minimum value (if the lower limit of the range is not reached) or the maximum value (if the upper limit of the range is exceeded) is set.

Examples

Dim FilStop As Double
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FILTer.GATE.TIME.STOP = 2E-8
FilStop = SCPI.CALCulate(1).SELected.FILTer.GATE.TIME.STOP

Related objects

SCPI.CALCulate(Ch).SELected.FILTer.GATE.TIME.STARt

SCPI.CALCulate(Ch).SELected.FILTer.GATE.TIME.STATe

SCPI.CALCulate(Ch).PARameter(Tr).SELect

Equivalent key

Analysis > Gating > Stop

Equivalent SCPI command

Syntax

:CALCulate{[1]-4}[:SELected]:FILTer[:GATE]:TIME:STOP <numeric>

:CALCulate{[1]-4}[:SELected]:FILTer[:GATE]:TIME:STOP?

Query response

{numeric}<newline><^END>

Example of use

10 OUTPUT 717;":CALC1:FILT:TIME:STOP 2E-8"
20 OUTPUT 717;":CALC1:FILT:TIME:STOP?"
30 ENTER 717;A