SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute

Object type

Method (Write Only)

Syntax

SCPI.CALCulate(Ch).SELected.FUNCtion.EXECute

Description

This command executes the analysis specified with the SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE object, for the active trace of the selected channel (Ch).

Examples

SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.FUNCtion.EXECute

Related objects

SCPI.CALCulate(Ch).SELected.FUNCtion.DATA

SCPI.CALCulate(Ch).PARameter(Tr).SELect

SCPI.CALCulate(Ch).SELected.FUNCtion.TYPE

SCPI.CALCulate(Ch).SELected.FUNCtion.DOMain.STATe

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:CALCulate{[1]-4}[:SELected]:FUNCtion:EXECute

Example of use

10 OUTPUT 717;":CALC1:FUNC:EXEC"