SCPI.CALCulate(Ch).SELected.LIMit.REPort.DATA

Object type

Property (Read Only)

Syntax

Data = SCPI.CALCulate(Ch).SELected.LIMit.REPort.DATA

Description

This command reads the stimulus values (frequency, power level or time) at all the measurement points that failed the limit test, for the active trace of the selected channel (Ch).

Variable

Parameter

Data

Description

Indicates the array data for failed measurement points (can be read out with the SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts object).

Data type

Variant type (Variant)

Examples

Dim FailData As Variant
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.LIMit.STATe = True
FailData = SCPI.CALCulate(1).SELected.LIMit.REPort.DATA

Related objects

SCPI.CALCulate(Ch).PARameter(Tr).SELect

SCPI.CALCulate(Ch).SELected.LIMit.REPort.POINts

SCPI.CALCulate(Ch).SELected.LIMit.STATe

Equivalent key

No equivalent key is available on the front panel.

Equivalent SCPI command

Syntax

:CALCulate{[1]-4}[:SELected]:LIMit:REPort[:DATA]?

Query response

{numeric 1},… ,{numeric N}<newline><^END>

Where N is the number of the measurement points that failed (can be read out with the :CALC{1-16}:LIM:REP:POIN? command).

Example of use

10 OUTPUT 717;":CALC1:LIM:REP:POIN?"
20 ENTER 717;A
30 REDIM B(1:A)
40 OUTPUT 717;":CALC1:LIM:REP?"
50 ENTER 717;B(*)