Property (Read Only)
Status = SCPI.CALCulate(Ch).SELected.RLIMit.FAIL
This command reads the ripple test result for the active trace (specified with the SCPI.CALCulate(Ch).PARameter(Tr).SELect command) of the selected channel (Ch).
|
Parameter |
Status |
|
Description |
The ripple test result |
|
Data type |
Boolean type (Boolean) |
|
Range |
Select from the following:
|
|
Note |
When the ripple test if set to OFF, False or OFF is always read out. |
Dim Result As Boolean
Result = SCPI.CALCulate(1).SELected.RLIMit.FAIL
SCPI.CALCulate(Ch).PARameter(Tr).SELect
SCPI.CALCulate(Ch).SELected.RLIMit.STATe
No equivalent key is available on the front panel.
:CALCulate{[1]-4}[:SELected]:RLIMit:FAIL?
10 OUTPUT 717;":CALC1:RLIM:FAIL?"
20 ENTER 717;A