SCPI.CALCulate(Ch).SELected.TRANsform.TIME.LPFRequency

Object type

Property (Write Only)

Syntax

SCPI.CALCulate(Ch).SELected.TRANsform.TIME.LPFRequency = Value

Description

This command changes the frequency range to match with the low-pass type transformation of the transformation function of the time domain function, for the active trace of the selected channel (Ch).

Examples

SCPI.CALCulate(1).PARameter(1).SELect
SCPI.CALCulate(1).SELected.TRANsform.TIME.LPFRequency = 1E5

Related objects

SCPI.CALCulate(Ch).SELected.TRANsform.TIME.TYPE

SCPI.CALCulate(Ch).SELected.TRANsform.TIME.STATe

SCPI.CALCulate(Ch).PARameter(Tr).SELect

Equivalent key

Analysis > Fault Location > Set Freq Low pass

Equivalent SCPI command

Syntax

:CALCulate{[1]-4}[:SELected]:TRANsform:TIME:LPFRequency

Example of use

10 OUTPUT 717;":CALC1:TRAN:TIME:LPFR 1E5"