SCPI.HCOPy.IMMediate

Object type

Method (Write Only)

Syntax

SCPI.HCOPy.IMMediate

Description

This command outputs the display image on the LCD display to the printer connected to the E5061B.

Examples

SCPI.HCOPy.IMMediate

Related objects

SCPI.HCOPy.ABORt

SCPI.HCOPy.IMAGe

Equivalent key

System > Print

When performing the operation from the front panel, the image on the LCD display memorized in the volatile memory (clipboard) (the image on the LCD display when the Capture (System) key is pressed) is printed. If no image is memorized in the clipboard, in the same way as the SCPI.HCOPy.IMMediate object, the image on the LCD display at the execution is memorized in the clipboard and then it is printed.

Equivalent SCPI command

Syntax

:HCOPy[:IMMediate]

Example of use

10 OUTPUT 717;":HCOP"