Method (Write Only)
SCPI.MMEMory.LOAD.CHANnel.COEFficient = Param
This command recalls the channel coefficient data of the active channel from the specified register.
|
Parameter |
Param |
|
Description |
Register |
|
Data Type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Note |
If no channel state has been saved in the specified register, an error occurs and the object is ignored. |
Dim Rgstr as String
Rgstr = "A"
SCPI.MMEMory.LOAD.CHANnel.COEFficient = Rgstr
SCPI.MMEMory.LOAD.CHANnel.STATe
SCPI.MMEMory.STORe.CHANnel.COEFficient
SCPI.MMEMory.STORe.CHANnel.STATe
No equivalent key is available on the front panel.
:MMEMory:LOAD:CHANnel:COEFficient {A|B|C|D}
{A|B|C|D} <newline><^END>
10 OUTPUT 717;":MMEM:LOAD:CHAN:COEF B"