Method (Write Only)
SCPI.MMEMory.STORe.CHANnel.COEFficient = Param
This command saves the channel coefficient data of the active channel specific to that channel only into the specified register (volatile memory).
|
Parameter |
Param |
|
Description |
Register |
|
Data Type |
Character string type (String) |
|
Range |
Select from the following:
|
|
Note |
If an instrument state has been already saved in the specified register, its contents are overwritten. |
Dim Rgstr as String
Rgstr = "B"
SCPI.MMEMory.STORe.CHANnel.COEFficient = Rgstr
SCPI.MMEMory.LOAD.CHANnel.COEFficient
SCPI.MMEMory.LOAD.CHANnel.STATe
SCPI.MMEMory.STORe.CHANnel.STATe
Save/Recall > Save Channel > Cal Only A , Cal Only B , Cal Only C , Cal Only D
:MMEMory:STORe:CHANnel:COEFficient {A|B|C|D}
{A|B|C|D} <newline><^END>
10 OUTPUT 717;":MMEM:STOR:CHAN:COEF C"