Method (Write Only)
SCPI.MMEMory.LOAD.LIMit = File
This command recalls the specified limit table file (file with the .csv extension saved with SCPI.MMEMory.STORe.LIMit), from the limit table for the active trace of the active channel.
Specify the file name with the extension. When you use directory names and file name, separate them with "\" (back slash), or "/" (slash).
|
Parameter |
File |
|
Description |
File name of limit table (extension ".csv") |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Note |
If the specified file does not exist, an error occurs when executed and the object is ignored. |
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.LOAD.LIMit = "d:\limit01.csv"
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.LOAD.LIMit = "test/limit01.csv"
SCPI.DISPlay.WINDow(Ch).ACTivate
SCPI.CALCulate(Ch).PARameter(Tr).SELect
Analysis > Limit Test > Edit Limit Line > Import from CSV File
:MMEMory:LOAD:LIMit <string>
10 OUTPUT 717;":MMEM:LOAD:LIM ""Test1/Limit01.csv"""
10 OUTPUT 717;":MMEM:LOAD:LIM ""D:Limit01.csv"""