Method (Write Only)
SCPI.MMEMory.STORe.FDATa = File
This command saves the formatted data array into a file in the CSV format (extension ".csv"), for the active trace of the active channel.
Specify the file name with the extension. When you use directory names and file name, separate them with "\" (back slash), or "/" (slash).
|
Parameter |
File |
|
Description |
File name in which you want to save the formatted data array (extension ".csv") |
|
Data type |
Character string type (String) |
|
Range |
254 characters or less |
|
Note |
If a file with the same name as the specified file name exists, its contents are overwritten. |
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.STORe.FDATa = "d:\trace01.csv"
SCPI.DISPlay.WINDow(1).ACTivate
SCPI.CALCulate(1).PARameter(1).SELect
SCPI.MMEMory.STORe.FDATa = "test/trace01.csv"
SCPI.DISPlay.WINDow(Ch).ACTivate
SCPI.CALCulate(Ch).PARameter(Tr).SELect
Save/Recall > Save Trace Data
:MMEMory:STORe:FDATa <string>
10 OUTPUT 717;":MMEM:STOR:FDAT ""Result/Trace01.csv"""
10 OUTPUT 717;":MMEM:STOR:FDAT ""D:Trace01.csv"""