SCPI.SENSe(Ch).DC.MEASure.CLEar

Object Type

Method (Write Only)

Syntax

SCPI.SENSe(Ch).DC.MEASure.CLEar

Description

This command clears the measurement data of DC monitor sweep end, for the selected channel ( Ch).

Examples

SCPI.SENSe(1).DC.MEASure.CLEar

Related Objects

SCPI.SENSe(Ch).DC.MEASure.ENABle

SCPI.SENSe(Ch).DC.PARameter

Equivalent Key

Meas > DC Monitor Setup > DC Monitor On Sweep End > Clear

Equivalent SCPI Command

Syntax

:SENSe{[1]-4}:DC:MEASure:CLEar

Example of use

10 OUTPUT 717;":SENS1:DC:MEAS:CLE"