Property (Read-Write)
SCPI.SYSTem.DATE = Data
Data = SCPI.SYSTem.DATE
This command sets/gets the date of the clock built in the E5061B. When you logged in the E5061B as standard user, an error occurs. Log in the user name of "Administrator" is required in case of Windows 10.
|
Parameter |
Data |
|
Description |
Indicates 3-element array data (date of the built-in clock).
The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
|
Range |
|
|
Resolution |
1 |
Dim Day As Variant
SCPI.SYSTem.DATE = Array(2012,12,24)
Day = SCPI.SYSTem.DATE
Dim Day(2) As Variant
Dim Ref As Variant
Day(0) = 2012
Day(1) = 12
Day(2) = 24
SCPI.SYSTem.DATE = Day
Ref = SCPI.SYSTem.DATE
System > Misc Setup > Clock Setup > Set Date and Time
:SYSTem:DATE <numeric 1>,<numeric 2>,<numeric 3>
:SYSTem:DATE?
{numeric 1},{numeric 2},{numeric 3}<newline><^END>
10 OUTPUT 717;":SYST:DATE 2012,1,1"
20 OUTPUT 717;":SYST:DATE?"
30 ENTER 717;A,B,C