Property (Read-Write)
SCPI.SYSTem.TIME = Data
Data = SCPI.SYSTem.TIME
This command sets/gets the time of the clock built in the E5061B. When you logged in the E5061B as standard user, an error occurs. Log in the user name of "Administrator" is required in case of Windows 10.
|
Parameter |
Data |
|
Description |
Indicates 3-element array data (time of the built-in clock). Data(0): Sets hour (24-hour basis) Data(1) :Sets minute. Data(2) :Sets second. The index of the array starts from 0. |
|
Data type |
Variant type (Variant) |
|
Range |
Data(0) :0 to 23 Data(1) :0 to 59 Data(2) :0 to 59 |
|
Resolution |
1 |
Dim Time As Variant
SCPI.SYSTem.TIME = Array(21,30,0)
Time = SCPI.SYSTem.TIME
Dim Time(2) As Variant
Dim Ref As Variant
Time(0) = 21
Time(1) = 30
Time(2) = 0
SCPI.SYSTem.TIME = Time
Ref = SCPI.SYSTem.TIME
System > Misc Setup > Clock Setup > Set Date and Time
:SYSTem:TIME <numeric 1>,<numeric 2>,<numeric 3>
:SYSTem:TIME?
{numeric 1},{numeric 2},{numeric 3}<newline><^END>
10 OUTPUT 717;":SYST:TIME 17,30,0"
20 OUTPUT 717;":SYST:TIME?"
30 ENTER 717;A,B,C