SCPI.SYSTem.UPReset

Object type

Method (Write Only)

Syntax

SCPI.SYSTem.UPReset

Description

This command presets the E5061B with the user settings. The command is executed regardless of the operation mode in preset state.

Examples

SCPI.SYSTem.UPReset

Related objects

SCPI.IEEE4882.RST

SCPI.SYSTem.PRESet

Equivalent key

Preset > OK

Equivalent SCPI command

Syntax

:SYSTem:UPReset

Example of use

10 OUTPUT 717;":SYST:UPR"