Property (Read-Write)
SCPI.TRIGger.OUTPut.POSition=Param
Param=SCPI.TRIGger.OUTPut.POSition
This command sets/gets the position of the External Trigger Output Port.
|
Parameter |
Param |
|
Description |
Sets/Gets (after or before measurement point) position of the output trigger. |
|
Data type |
Character string type (String) |
|
Range |
Select from either of the following: |
|
Preset value |
"AFTer" |
Dim TrigPos As String
TrigPos="BEFore"
SCPI.TRIGger.OUTPut.POSition=TrigPos
Trigger > Position
:TRIGger:OUTPut:POSition {AFTer|BEFore}
:TRIGger:OUTPut:POSition?
{AFT|BEF}<newline><^END>
10 OUTPUT 717;":TRIG:OUTP:POS AFT"
20 OUTPUT 717;":TRIG:OUTP:POS?"
30 ENTER 717;A$