Property (Read-Write)
SCPI.TRIGger.OUTPut.POLarity=Param
Param=SCPI.TRIGger.OUTPut.POLarity
This command sets/gets the polarity of the pulse generated from the External Trigger (Output).
|
Parameter |
Param |
|
Description |
Sets/Gets polarity of the pulse generated by the output trigger. |
|
Data type |
Character string type (String) |
|
Range |
Select from either of the following:
|
|
Preset value |
"POSitive" |
Dim TrigPol As String
TrigPol="NEGative"
SCPI.TRIGger.OUTPut.POLarity=TrigPol
Trigger > Polarity
:TRIGger:OUTPut:POLarity {POSitive|NEGative}
:TRIGger:OUTPut:POLarity?
{POS|NEG}<newline><^END>
10 OUTPUT 717;":TRIG:OUTP:POL POS"
20 OUTPUT 717;":TRIG:OUTP:POL?"
30 ENTER 717;A$