Property (Read-Write)
SCPI.TRIGger.SEQuence.EXTernal.DELay = Value
Value = SCPI.TRIGger.SEQuence.EXTernal.DELay
This command sets/gets the time that it takes from receiving the trigger to starting the measurement when the trigger source is external.
|
Parameter |
Value |
|
Description |
External trigger delay time |
|
Data type |
Double precision floating point type (Double) |
|
Range |
0 to 1 |
|
Preset value |
0 |
|
Unit |
s (second) |
|
Resolution |
1E-5 |
Dim Extdel As Double
SCPI.TRIGger.SEQuence.EXTernal.DELay = 0.05
Extdel = SCPI.TRIGger.SEQuence.EXTernal.DELay
Trigger > Trigger Delay
:TRIGger[:SEQuence]:EXTernal:DELay <numeric>
:TRIGger[:SEQuence]:EXTernal:DELay?
{numeric}<newline><^END>
10 OUTPUT 717;":TRIG:EXT:DEL 0.05"
20 OUTPUT 717;":TRIG:EXT:DEL?"
30 ENTER 717;A