Property (Read-Write)
SCPI.TRIGger.SEQuence.EXTernal.SLOPe=Param
Param=SCPI.TRIGger.SEQuence.EXTernal.SLOPe
This command sets/gets the polarity of the External Trigger (Input).
|
Parameter |
Param |
|
Description |
Sets/Gets polarity of the external trigger (input). |
|
Data type |
Character string type (String) |
|
Range |
Select from either of the following:
|
|
Preset value |
"NEGative" |
Dim InputTrigPol As String
InputTrigPol="NEGative"
SCPI.TRIGger.SEQuence.EXTernal.SLOPe=InputTrigPol
SCPI.TRIGger.SEQuence.EXTernal.DELay
Trigger > Ext Trig Input
:TRIGger[:SEQuence]:EXTernal:SLOPe {POSitive|NEGative}
:TRIGger[:SEQuence]:EXTernal:SLOPe?
{POS|NEG}<newline><^END>
10 OUTPUT 717;":TRIG:EXT:SLOP POS"
20 OUTPUT 717;":TRIG:EXT:SLOP?"
30 ENTER 717;A$